Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

7 Guidelines for Cable Installation
The proper installation of a cable is key to get the maximum performance and service life. Simple, easy to-follow guidelines can make the difference between thousands and millions of cycles of service life. In this guide, review 7 quick rules for proper cable installation in your next application.

Before installation, many professionals and cable manufacturers will claim that it is necessary to allow for at least 24 hours for cables to be “relaxed,” or “shaken out.” Relaxation time is a luxury these days – most engineers are faced with increasingly tight deadlines, reduced resources, and a multitude of different responsibilities. We relax to de-stress from hectic work and family lives. Likewise, many manufacturers recommend cables to be relaxed for installation to release stress from storage on a spool or reel before installation.
continuous-flex cables in cable carrier 1.1 Chainflex® continuous-flex cables do not have to be relaxed prior to being installed into a cable carrier.
To allow for more relaxation time for the engineers and installation team, the igus® cable experts agree that a Chainflex® cable should be cut to the desired length and installed directly into a cable carrier. Our 25 years of experience in cable manufacturing and installation allows us the confidence to say that if properly designed (see the 7 seven key design features of a continuous-flex cable here), it is not necessary to waste time laying or hanging cables before their installation. Instead, use the following guide to ensure the performance of your cables quickly and easily.

  1. Unspool cables properly- always allow spools to roll while unspooling cables. Do not pull cables from the flange, or uncoil from the top of the spool. This can cause unnecessary stress to cables.

  2. Check the jacket materials of different cables - in some instances, different jacket materials can stick together and cause abrasion. Check to see if your cables’ jacket materials are intended for use inside a cable carrier, or for use with corresponding jacket materials. Abrasion of jacket materials can sometimes be prevented with interior separation.

  3. Cut to the proper length, and lay directly inside the cable carrier. Ensure each cable is long enough for proper connection and strain-relief (see guideline #7). Laying cables is the preferred method for placing inside a cable carrier, especially cables that have already been harnessed with connectors. Cables can also be carefully pulled into the proper positioning in the cable carrier if necessary. Avoid any twisting of the cable while placing into the carrier.

  4. Ensure every cable has room to move freely during movement of the cable carrier. Be sure each cable has plenty of room to move while in operation. This will maximize the service life, and reduce risk of abrasion and other common cable failures.(Learn more about common cable failure modes here)

  5. Take the time to be sure that cables rest in the neutral axis of the cable carrier, especially while operating at the carrier’s maximum bend radius. When the carrier is bent, there should be no tensile forces exerted on the cable.

  6. If cables/hoses of varying diameters are being installed, utilize interior shelving or separators. This will prevent tangling. There are two easy cable distribution rules to follow to see if interior separation is needed. The first states that If the diameters of the cables, D1+D2 are greater than 1.2 x the inner height of the cable carrier, no separation between the two cables/hoses is necessary. If the diameters of cables D1+D2 is less than or equal to the inner height of the cable carrier, use vertical separators or horizontal shelf to prevent crossover/abrasion. more resilient material will gradually wear down the softer jacket, leading to failure.

  7. Use strain relief at both ends of cables. There are a number of strain relief options, including mounting brackets, tie wrap plates, etc. Proper strain relief keeps the length of cable inside the carrier fixed at all times. In certain cases, strain relief may only be necessary at the moving end of the cable carrier.
installing Chainflex continuous-flex cables A continuous-flex cable can removed from the spool and immediately installed.

Useful Links and Tools



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302