Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Reliable over long travels

Cable carrier system with aluminum guide trough

Cable carriers are pushed to the limit and so are able to prove their technical and economic strengths when it comes to crane applications. In long travel applications, aluminum guide troughs are used to guide the cable carrier.

In an existing project, a crane facility in a cement factory was equipped with made-to-measure cable carrier systems for a fully automated storage and removal system used for clearing sludge. Proven in long travel applications, chainflex® continuous-flex cables and aluminum guide troughs are also used.
cable carrier with continuous flex cables The following chainflex® continuous-flex cables are used: motor cables, control cables, data cables, and bus cables.
cable carrier guide-trough system for long travels Guide-trough system for long travels

Demands on the aluminum trough

The crane track has a length of 105 ft (32 m). The trolley speed is at 3.3 ft/s (1 m/s), the crane speed is at 4.4 ft/s (1.3 m/sec), and the lifting speed is 3.3 ft/s (1 m/s). The lift height is equal to just over 26 ft (8 m). The crane also uses aluminum trough which, together with the cable carrier, makes a compact and space-saving system.
readychain® cable carrier View from above of the complete system, including aluminum trough

Basic trough package

The basic package of the guide trough consists of just four parts: trough wall, glide bar, clamping shoe and fastener. The trough wall is made of extruded aluminum and is light, stable, resistant to sea water and suitable for demanding environments.
cable carrier aluminum guide trough The aluminum guide trough is stable against forces from all directions

Additional product information

More applications examples from different industries



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302