Root ball transplanter
Root ball transplanters are indispensable tools for tree nurseries and for garden and landscaping businesses.

Excellent polymers improved by precisely harmonized states of strengthening materials and solid lubricants, tested a thousand times and proved a million times - that is iglidur®.
igus® engineers develop more than 100 new plastic compounds every year, test the maintenance-free plain bearings in more than 3,500 experiments each year and have built up a comprehensive database on tribiological properties of the polymers in the past years.
Root ball transplanters are indispensable tools for tree nurseries and for garden and landscaping businesses.
In this case, the use of igus® products is not only advantageous from a technical, but also from a financial point of view when compared to competitive products.
A builder of technical brush making machinery known world-wide, uses plain bearings from the igus® product range.
Plastic plain bearings in process engineering: Completely maintenance and lubricant-free.
Due to their low weight, iglidur® Q plain bearings were used in place of bronze bushings for the spring suspension of the racing car.
The replacing of the steel bearings with special plain bearings made of plastic has caused a clear weight reduction.
Among full-suspension mountain bikes light polymer plain bearings are used to handle severe stresses at the dropouts of the rear suspension.
Hinges for heavy doors in mega yachts: fully maintenance-free.
Seawater-resistant, wear-resistant polymer plain bearings are used in the new generation models of yacht building instead of self-made roller bearings.
Due to the excellent wear resistance and freedom from lubrication, iglidur® X6 bearings are used in wafer baking tongs.
Golfcraft golf trolleys made of carbon and aluminum - lightweight and foldable.
The driver lies on this vehicle with his armed stretched out and head facing forward.
In this car-trailer, an igus® flange bearing made of iglidur® Z replaces the previously used phosphor bronze bearing.
igus® plastic plain bearings are used here in the shock absorber of an excavator seat.
Moisture and extreme temperature fluctuations often lead to undesirable expansion of the component parts.
Plain bearings are used, made of iglidur® A500, an FDA-compliant high-temperature material.
This device is used for folding letters. The folding operation in a small space reduces the frame sizes of folding machines.
This machine can scan books fully automatically, with no human intervention required.
The components used must be suitable for use with food, which is why the design engineers decided in favour of xiros® ball bearings.
These fully functional steam locomotives have been built to a scale of 1:11.
This machining results in lost of wood chips and dust, of course, which would stick to lubricants.
This design was first used to deal with problems of clearance and friction. With iglidur® G plain bearings, however, these problems were eliminated.
The bearings of the ice screw must be insensitive to water and dirt, as well as thermally insulated.
Lightweight components are particularly important here to ensure as little energy as possible is required for movement.
Plain bearings from igus® are used for the movement of the front and rear wheels. Thanks to them, there are no problems with wear or corrosion.
This electric wheelchair also makes use of the properties of igus® plain bearings.
The bicycle pedal presented here responds to the ergonomic and biomechanical needs of cyclists.
Here, igus® plastic plain bearings have replaced classical roller bearings and stand up to environmental influences such as dirt and corrosion.
Silver Award at manus® 2011: String trimmer-cutting disc of PRODULEX UNIPESSOAL LDA, Portugal
This valve is used for filling ice-cream containing pieces of fruit in fully automatic industrial packing machines.
This small vehicle adheres firmly to surfaces with its magnetic wheels, to inspect welding joints.
This manus® contribution also shows an exceptional off-road wheelchair, the "Quadrix".
In this prosthesis for pneumatic knee joints, iglidur® J piston rings replace the previously used PTFE guide bands.
This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.
With this hand tool for the rolling and repairing of threads, the bearing support of the profi led roller is particularly important.
This manus® contribution is concerned with the cost-effective increase in production and process reliability for manual assembly using low-cost automation.
Bronze Award at manus® 2011: Hand prothesis of Vincent Systems GmbH, Germany
This machine is used to pack products in blister film.
A conventional material in an unusual application: This bike frame is entirely made of wood.
Here, the honey is being loosened from the combs. For this, the honeycombs are pierced with needles.
This solar system can be installed either on its own or in combination with a wind turbine.
This information board is exposed to the weather and the forces of nature all year round.
This inspection robot was developed especially for use in pipelines.
By using iglidur® W300 plain bearings, reliability can be increased. The previously used ball bearings had to be oiled regularly, which is not the case with iglidur® bearings.
Since temperatures of several hundred degrees Celsius occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures.
Another newly developed dolly for camera movement is the subject of this manus® contribution.
This folding trailer “Tyligo” is extremely flexible and can be used to transport all kinds of things.
Provides a seat without taking too much room away from pedestrians: this is possible with the „Sitty“ folding seat.
To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.
The various work processes like aluminum etching are sometimes done with extremely aggressive materials.
The high stressing through the three-shift operation and the shocks caused by the moving parts were crucial for the application of igus® products.
The main concern when designing the bearing support for this record player turntable was silent and low-vibration movement.
The exact positioning is important here, which is ensured by the combination of several igus® products.
This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.
This doll is used for representing maritime signals and originated from a marketing project in collaboration with a doll builder.
This pagepulltester is a high-precision measuring instrument for the bookbinding industry.
This fully functional hydraulic excavator was copied on a scale of 1:14.5.
Model train enthusiasts will enjoy this Rhätische Railway locomotive for a long time to come.
The stones used can weigh anything up to 4,000 kilogrammes. This means a heavy-duty load for all the components used.
This solar thermal power plant also obtains energy from the rays of the sun, without fossil fuels.
The manus® contribution submitted here is the new development of a patient lift for ambulances for transporting patients who are able to sit in the vehicle.
In this application, metallic ball bearings and DU bushings have been replaced by lighter iglidur® flange bearings.
xiros® ball bearings from igus® are used in this planetary gearbox that is used in wind turbines.
This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.
This machine is used for loading and unloading of boxes at an automated warehouse.
The suspension pins in this racing car were previously guided without bearings.
An extremely light weight is the most important criterion when constructing a racing bike brake.
This contribution to the manus® competition – a robot gripper – is extremely flexible.
Special Award at manus® 2011: Robot Head of Archimedes Solutions GmbH, Germany
With this application, salami is cut into slices. As with all applications in contact with food, here too lubricants cannot be used.
Here, sanitary elements in the bathroom unit are installed with igus® products.
This machine weaves and prints terry cloth hand towels.
All igus® products used are maintenance- free, giving the machine a long service-life.
The „ConCut“ is a CNC-controlled cutting system for confectionary products.
A tarp is lowered slowly over the car, so that at first only the outlines are visible; then the tarp is cut by the special mechanism and the car is presented to the public.
This cutting mechanism is used in the beverage industry. Several igus® products were used here.
Children are especially prone to squeeze their fingers in glass swinging doors. This safety door prevents that, because it „gives“.
This innovative sledge allows people to ski sitting down. The sledge is steered by the feet and tilted by the hands.
This exceptional sporting equipment makes bombing down a ski slope like riding a bicycle.
iglidur® plain bearings and thrust washers are shown here in the service of art.
This solar system can be installed either on its own or in combination with a wind turbine.
For solar systems to retain their entire performance capacity, they have to be cleaned at regular intervals, particularly in sandy regions.
Previously, metal bearings and linear guides were used, which rusted quickly and therefore required frequent maintenance.
No matter how much the sun shines: these sunshades ensure pleasant light conditions within the building.
This special wheelchair allows people who can only walk with diffi culty to go to the beach.
This motor is to drive deep-sea robots even at 6,000 metres under the sea.
Gold Award at manus® 2011: Machine for frying Spanish omelettes of Carmelo Lagunas Escudero, Spain
This equipment is used in the food industry. The baked goods are separated on these chains.
In this pedal boat, the moving parts of the drive mechanism must be mounted free of lubricants, since the screw is in the water.
In this application, plain bearings made of iglidur® Z replace a ball bearing and a needle bearing in a superimposed transmission.
Seawater is a very corrosive environment on account of its high salt content. Components that are exposed to the water must withstand it.
This fully automatic page turner for people with disabilities can automatically turn the pages of many newspapers, magazines, folders, exercise books and the like.
This application shows a conversion kit for the suspension in three-wheeled motorcycles.
igus® thrust washers and flange bearings were used for the new design. They made the elaborate milling of the base plate unnecessary.
This equipment can package various industrial products, with any materials.
the armrests of this chair are adjustable, to accommodate the needs of the individual user.
In this exercise equipment, vibrations are specifically used to build up muscles.
Any movement that is to be performed here must be lubrication-free, executed free of wear and, if wear does occur, it must be free of heavy metals, etc., that could give distorted results in the chemical analysis.
The use of iglidur® bearings quadrupled the service life of the machine. It made it possible to save almost 300 mechanic-hours plus ca. 8 tonnes of cotton wool.
For the gripper bracket for screws in automatic screwing devices – previously a job done by steel cheeks.
This application creates new possibilities in steel construction, shipbuilding, cable cars, plant engineering or in general mechanical engineering.
With this snowboard, the “Twistboard”, both parts are connected via an axially aligned joint.
The model of a "chemical accident robot" was developed by four students.
Changeover to corrosion-resistant, lightning-resistant and insulated plastic plain bearing in the entire airplane system.
The unusual design for a recumbent bicycle has got what it takes: cordless screwdrivers are used here to drive it.
Light, corrosion-proof and economical slide bearings are needed for this application.
The edge load is frequently a deciding factor for or against the use of bearings particularly in axle bearings for agricultural vehicles.
Rheinische Fachhochschule (technical college) in Cologne: Reduction of friction when the ball gripper's camera arm is extended.
iglidur® plastic plain bearings in cranes used in commercial and private marinas and also by private boat owners to haul the boats out of the water.
Chemical-resistant and corrosion-free: maintenance-free polymer plain bearings in catering kitchen appliances.
The low demand for space and freedom from corrosion of iglidur® J plain bearings qualified them for use in this model.
Wind, sand and sun: Plastic plain bearing for solar technology
Short linear strokes and changing pivoting angle under various impact loads are the demands on plain bearings made of iglidur® G.
iglidur® G bearings have proved their worth by their freedom from maintenance and lubricants, the good abrasion resistance under high loads and the resistance to media.
Maintenance-free guide and bearing in arm and leg rest on the dialysis chair.
Plain bearings made of iglidur® G have been in use since 2001 without lubrication and without any significant proof of wear in the very harsh ambient conditions of construction machinery.
The completely dry operation and the thereby associated dirt-resistance is very important in the direct application in seeds.
International robotics competition: Technical University of Chemnitz gears up to meet international competition.
Plain bearings in the packaging industry against friction and wear.
Plastic plain bearing in almost oxygen-free atmosphere: World record for flight altitude in a hot-air balloon.
Pivot and rotate with plastic plain bearings - New glass lamellae system / Adjustable facade for the service center of an automobile manufacturer.
Polymer plain bearings find their way increasingly into traditional organ building.
For top-quality French fries - The lubricant-free polymer bearings in a filtration device for fry fat contribute to maintain food quality.
Bearings made of the "iglidur Q" material cope with high loads just as well with various pivoting angles and are thus ideally suitable for the application in the "Zoob" electric scooter.
Always at your service ... and at the same time cost-efficient; polymer bearings guard against downtimes on the long term.
Pivot and rotate under pressure - High-performance polymers in wood working.
On the winning path - Control unit for high-tech mountainbikes profits from plastic plain bearings.
Patient's welfare in focus - How polymer bearings improve an artificial joint.
Plastic plain bearings in application in machine tool manufacture at Deckel Maho Gildemeister.
Precise and durable - Polymer bearings for novel leather splitting machine.
For increased service life - Low-cost angular sensor with special bearings in printing machines.
Sought by Mr. Clean - The lubricant-free bearing system is highly recommended for the food and hygiene industry.
Wear inspection - How bearings assist in the inspection of pneumatic seals.
Compensatory special parts tolerance in rugged agricultural machinery construction.
New solutions for fitness equipment save production costs and assembly times.
The extreme resistance to chemicals was decisive for the application of iglidur® bearings.
iglidur® G plain bearing in hydraulic cylinder for construction machines.
We can offer a significant advantage in racing by the enormous weight reduction achieved by iglidur® W300 bearings.
On the ecoflow pumps, "iglidur® X" plain bearings of various sizes are used.
In this application, the resistance to edge loads is of great significance besides the complete freedom from maintenance and lubrication.
The motor-powered swiveling LED wings are adjusted with the aid of iglidur® JVFM-0810-08.
The complete freedom from maintenance in areas of extreme dirt accumulation distinguishes the iglidur® J plain bearing.
Stabilization of the robot's undercarriage without loss of flexibility with igus® plain bearings.
The iglidur® G plain bearings distinguish themselves by their wear resistance and the suitability for real dry operation in this packaging machine for polishing cloth.
Besides the high chemical resistance, the iglidur® J plain bearings offer a maintenance-free dry operation in this application.
Besides the high chemical resistance, the iglidur® J plain bearings offer a maintenance-free dry operation in this application.
In this application, the iglidur® J plain bearings replace the lubricated ball bearings.
By the application of iglidur® RN plain bearings, the drive energy required for the bottle washing machine could be significantly reduced.
Extreme chemical resistance in small lots was decisive for the application of iglidur® X plain bearings in almost all flanged ball valves of the company Pister.
The crimpers in hose packaging machines often reach temperatures of 160°C and above in continuous operation.
The maintenance-free polymer bearings are used in rust-proof roller chains, which are employed to drive main and auxiliary equipment.
The high edge load in particular is the main reason for the use of iglidur® G plastic thrust washers.
Quick, straight, precise: this is how the requirements in sheet metal machining can be summarized. Sophisticated straightening technology makes all this possible.
iglidur® Z plain bearings in a roller coaster at Six Flags Theme Park have significantly reduced costs.
Now freedom from corrosion is an important argument for the application of iglidur® G plain bearings in ship fittings.
High wear resistance and freedom from maintenance are the main reasons for the application of iglidur® plain bearings.
An oil-free operation of the engine could be ensured only by the use of plastic plain bearings.
Freedom from lubricants and corrosion of iglidur® G are ideal for the application.
The enormous cost advantages compared to standard commercial metallic rolled bushings as well as an extreme resistance to wear distinguish iglidur® D.
Always on the mark - Plastic bearings for young engineers of the TU Munich.
Multi-step, single-flow underwater motor pumps with integrated non-return valve.
The reduction of the drive power for bottle washing machines was an important achievement of the iglidur® RN plain bearings.
Vocational school in Burgdorf-Lehrte: Conversion of the gear drive into belt drive in an existing robot .
Lubrication-free tribopolymers in extreme application - Packaging unit for profiles.
Egg on four wheels - How rod end bearings and plastic bearings make a hydrogen-powered vehicle mobile.
Dust-repellant and maintenance-free: The tough rod end bearings and spherical bearings do a sturdy job in the special-purpose municipal vehicles.
Gold at manus® 2007: Autosplit D3 splitting machine
Maintenance-free track accuracy
No lubricants in food sector
Precise and ergonomic
Hot and quick
Robust under high forces
Long-lasting and cost-effective
The used bearing must be lubricant-free, because silica sand is used here.
The plain bearing used has a low frictional resistance and is low maintenance and lubricant-free.
Can be handled alone
Easy and durable
Saves costs and better
Less wear
Corrosion-proof in sea water
Affordable and long-lasting
High load capacity and durable
Cost-effective and maintenance-free
Economical even when exposed to heat
Quiet and low friction
Resistant and long-lasting:
Over 170,000 Euro of benefits were able to be achieved by using polymer plain bearings
Secure under high forces: maintenance-free plain bearings made of iglidur® Z can withstand extreme loads.
In conventional solutions, while cleaning, the lubricant on the bearings is washed away or the bearings are even rinsed to get rid of the dirt particles.
In a newly designed mechanism, the conventional roller ball bearings were replaced by iglidur® plastic plain bearings.
Consistent application of igus® plain bearings in the aircraft design in fiber composite honeycomb-
sandwich construction.
Enhancement of service life, machine availability, stability and carrying capacity by the application of iglidur® in rollers on mini excavator.
Over 30 iglidur® plastic plain bearings assist to satisfy these requirements.
In this scooter, the steering was newly designed with igus® polymer plain bearings.
Bearing materials marked by special properties such as low coefficients of friction in dry operation, resistance to chemicals and low humidity absorption in equal measure are best suited for the application in high-tech beverages bottling plants.
Adjustable desktops in workplaces for the handicapped.
The problem of the design was in the limited installation space by the combination of two movements independent of each other and the high mechanical stressing.
Here an iglidur® polymer slewing ring bearing is used, which is distinguished by its low weight.
A problem that vexed the designers was the total weight and the occurring leverages. Here the weight should be saved.
In this tool presetting device, DryLin® guide carriages made of iglidur® J200 are used as measuring carriages. They contribute toward the attainment of a precision and repeat accuracy of +/- 0.1 mm in the application.
Veneer jointing
machine ACR Speedstar: Cost advantages through polymer plain bearings.
iglidur® G is the problem solver in this rotor head The rotor blades rotate about 400 times per minute and thereby execute oscillating motion with maximum 30°.
A UV radiator unchanged for 10 years was reconstructed and improved in the details. The iglidur® Z flange bearing reduces here the costs and the amount of maintenance.
By the almost wear-free bearing assembly that withstands a high pressure at the same time, this push-rod drive chain was optimized in line with the market.
By the use of iglidur® bearings, the cylinder is completely maintenance-free, and the weight could be reduced by about 10% of the original.
The universal joint presented here is, contrary to the common universal/cardan joints, not only designed for the transmission of torsional forces.
The backrest adjustment is implemented with DryLin® products, the headrests are mounted on the backrest with plastic plain bearings made of iglidur® G.
iglidur® X was selected as glide material for the guide of the piston rod due to the adequate resistance to temperature and moisture.
The hinge elements and cam rollers of the ramps are inserted with two iglidur® Z plain bearings respectively.
The motion of the driving rod of an organ should be utmost noiseless and smooth-running.
A bearing was sought for the following application: Hot frying oil up to 220° C, food safe. Solution to the problem: iglidur® A500 bearings.
Here the challenge in the design was that the bearing of the group of components for the application in the measuring medium water had to be designed.
In order to fulfill the bearing system's manifold requirements, the igus® bearings are used in the standard-production application.
The availability of the application even at above 100°C temperatures was guaranteed by the application of plastic plain bearings made of iglidur® X.
By the modification of the plain bearing partner plastic-metal into plastic-plastic, a conversion in the integral design was possible by the use of plastic components.
A novel external load system for helicopters required a low weight, high reliability with simultaneous weather resistance and freedom from maintenance.
By the application of a novel design, which feature an individual element made of iglidur® RN56 as the core piece, the technical requirements could be achieved at clearly reduced costs.
The application of an iglidur® plain bearing on the outer side of the pin was the main new aspect of the design.
By the use of igus® plain bearings, no notable clearance or abrasion was recognizable even after a long service life.
By a modified function system and the use of plastic bearings, a completely new generation of control wheels is developed, which is maintenance-free and low priced.
Automatic lock for a convertible top: By the use of the calibratable igus® flanged bearing, the maximum axial clearance could be lowered from 1.5 mm to 0.5 mm.
By the new arrangement of the plain bearings, the drive wheels of the transport vehicle could utilize the rotary movement of the individual bearing to guide the front wheels accurately through the track of the unloading station.
In the fulfilling of all requirements, the use of a pair of plastic bearings with elastic flange played the crucial role, which enabled the clearance-free installation of the locking hook.
Wheel mount handling for automobiles: Since about a year in daily use, the wheel mount handling system gives no trouble to the customers.
The advantages of using the bushing are: top-quality products, quick installation, long-lasting service life (2 million switching cycles) and the exceptional ruggedness.
The bearings have been installed about a year ago and since then operate free of troubles in the manufacturing.
Costs have been saved in mounting by the use of iglidur® plain bearings.
Ball bearing assemblies are very precarious due to the lubricant particularly under water. Stainless steel guidances cannot be considered due to the high costs. Plastic is used also for hygienic reasons.
The bearing tolerances could be clearly enhanced by the machining of the inner diameter of the iglidur® P polymer plain bearing.
Application of polymer plain bearings in a tire cord machine ensures stability
The application of Drylin® linear housings and iglidur® G plain bearings enable the centering pin to have a clean and easy drive up.
These igus® bearings look particularly suited for the specified application, as they are resistant to water, dirt and temperature and are also maintenance-free.
The main requirements of this application are: High dynamic accuracy, low weight with high stiffening and high availability in 3-shift operation.
An injection-molded part was created by igus® and used in the existing housing shell. Now it's been working for five years.
Testing devices for sintered parts: A lubricant-free linear guide (liquid pollution) should be guaranteed.
Pivot arm in injection-molding machines mounted with plastic plain bearings: With the simple plug-in installation and the adjustable collar, it was possible to abandon the highly complex bonding mechanism.
Plain, spherical and linear bearings made of plastic help to improve mobility and the quality of life
In the case of these gate drive units, different products from all the igus® divisions are used.
Exhaust valve on CNC drilling and milling machines
The suitability of iglidur® G plain bearings in pedal and lever bearing assemblies was proven in a test.
The plain bearings in the components are constantly exposed to air containing acid.
Replacement of metal bearings in concrete drilling and concrete sawing machines.
Boat motor lifting device and inner boom roll-up device equipped with plastic plain bearings.
Complete freedom from maintenance and stick-slip-free movement are the prerequisites for use in office chairs.
The reasons for using plastic plain bearings in this dialysis machine are the physiological safety, the abrasion resistance under high loads and the chemical resistance.
Printer and plotter - low drive forces, low sliding friction coefficients.
The plain bearings must withstand static radial loads of 25 N/mm² at temperatures of 170°C - 200°C.
Overhead conveyors for transporting packaged goods within the factory are used to transport a wide variety of goods.
The needle bearings previously used had to be serviced or replaced every few years.
Widely different sliding speeds - no problem with polymer plain bearings.
Loads up to 2000 N at temperatures of up to 250 °C characterize this application.
In the extremely chemically aggressive environment of semi-conductor production, metal plain bearings were regularly replaced after 2 to 3 weeks. Using iglidur® X plain bearings, the bearing point could be operated for years without problems.
Low wear on a wooden chair thanks to iglidur® A200 flange bearings.
iglidur® G plain bearings of different sizes are used on this equipment.
These sensors are used to prevent the blocks on the individual cranes from moving.
In drilling and sowing machines, the plain bearings are exposed to extreme levels of dirt, weathering and shock loads.
Due to their lower weight and better suspension qualities, the company switched to igubal® rod end bearings.
Thanks to iglidur® plain bearings, the company was able to reduce its costs by 93%! The assembly times were reduced by 10 minutes.
Requirements: fluctuating ambient temperatures, use in steam pipes with steam temperatures of 135 °C, use in acid and alkali tanks.
Due to the aggressive paper dust, the sintered bearings used before clogged up very quickly.
Vibration caused by the rotating wheel had to be dampened and the bearing assembly had to be corrosion resistant in order to withstand strong fertilizers and dew dampness in the grass.
The iglidur® plain bearings are used here in various bearing points.
This roller table represents a possible iglidur® D application, where it is a matter of the lowest possible drive forces.
Various plastic plain bearings are used on the different articulated joints of this multifunctional wheelchair.
A wheelchair ramp with plastic plain bearings was designed and installed at the front entrance of a low-floor bus.
Compared to the metal plain bearings first used, the better vibration dampening of iglidur® X reduced the noise of the cutter head.
The load on the bearing is around 10 N/mm², approx. 1000 cycles are performed per day.
Used in difficult conditions: vibration, random forces, sudden shocks and cold, wet snow.
The plastic bearings used do not need any oil and remain functional and clean. The performance of the plastic is not affected by extreme temperature fluctuations (hot and dry, cold and wet).
The bearings in this chain conveyor must be able to run dry, yet also come into contact with aggressive coolants and metal powders.
A special size bearing was developed so that it fits into the existing bearing without hindering the wall thickness.
The system uses an electromagnetic drive (plunger coil), which enables the required air pressure to operate piston and cylinder.
iglidur® W300 plain bearings are used here as a replacement for recirculating ball bearings.
The baking ingredients can easily settle in the mixer's catch and make it stick. iglidur® J is made of plastic and is therefore resistant to dirt and chemicals.
The telemark bindings kept on breaking and failing. A sturdy, maintenance-free product was able to be achieved using the iglidur® plastic bearings.
To prevent static charges on the bobbins, electrically conductive bushings are used in textile machinery construction.
iglidur® polymer bearings in variable intake systems.
iglidur® plastic plain bearing in the disc brake caliper of a utility vehicle
iglidur® plastic plain bearing in the convertible top system.
iglidur® plastic plain bearing in the steering system of a utility vehicle.
In order to keep the production costs and expenditure as low as possible, the application of non-variable parts is of great significance. The compromise between stability and flexibility could be solved by the aid of iglidur® plain bearings from igus®.
The bearings from igus® were decided because they are maintenance-free and cost-effective and absolutely simple to handle.
Application of a high-value spindle lift table with steep-threaded spindle, linear guide systems and igubal® spherical bearings.
The main tasks of the gripper arm were simple travel movements, light design, as well as the largest possible operating range.
DryLin® trapezoidal leadscrew nut in a sheet metal forming machine.
Plastic instead of recirculating ball bearings - DryLin® linear guides for machine deburring
Maintenance-free polymer bearings in mobile and stationary saw mills.
DryLin® linear guide systems provide for compact and thereby highly flexible handling devices.
DryLin® plastic plain bearings in an inspection device for offshore drilling riser
An engraving machine with igus® products, as final project work after four years of advanced education in automation technology.
Application of DryLin® high-temperature bearings in bag forming, filling and sealing machine for the sealing bar bearing
DryLin® in a champagne bottle
sealing machine in the filling technology.
Using DryLin® T linear guide and iglidur® PRT slewing ring bearings, the movement under the press and the pivoting of the parts to be assembled is mastered.
Automatically aligning the photovoltaic tracking systems to the position of the sun with the aid of lubricant-free plastic plain bearings produces a particularly high efficiency.
Since the clamping stars in this bottling plant were equipped with polymer bearings, the service life has almost doubled.
On these horizontal forming, filling and sealing machines, the total freedom from maintenance over the machines' entire life cycle was particularly important for the customer.
Initiated by Sachs Bikes, Norbert Staffend started with a focus on "motorized two-wheeler" in the student project. The result was this pure and elegant e-scooter
The Shell Eco-Marathon is the largest energy-efficiency competition and is aimed at student teams from across Europe.
Rugged liquid manure tank trucks are used for the economic distribution of biogas manure. In the steered pendular axles, lubricant-free polymer bearings defy all adverse conditions.
This project is a study module for the development of a model airplane. iglidur® bearings were used for mounting the aileron.
igus® contact+49 (0) 2203-9649-0Send e-mail to igus®
myigus myCatalog3D-CADOnline catalogNews 2013Product finder plain bearingsProduct finder piston ringsProduct finder for semi-finished productsLifetime calculationApplication examplesEmail the product expertInquiry/orderQuickSpecPart No. searchShaft inquiryCatalogs/samplesDownloadmanus® Competition
Terms and Conditions Imprint General Information Data Privacy Protection Declaration