In the retrofit process, now all axes of a 6-axis robot were fitted with multi-dimensionally moving energy chains®. The complete robot accessory package includes not only the 3D chains that protect and compactly guide cables and tubes in all movements, but also fiber rods for a directed pretension, as well as adapters, protectors and a chain for rotary motion. Since then, there has been no more downtimes.
"The core of our technical research center is a robot that is constantly in use," says Martin Weber of the Wandres GmbH micro-cleaning, Buchenbach-Wagensteig in the southern Black Forest. The company specializes in the development and production of brush and air-driven cleaning systems. The safe and gentle removal of dust, fibers and minute particles on surfaces is a prerequisite for many manufacturing processes to produce high quality products. "This is especially true for the automotive industry. The highest quality requirements prevail here," says Weber. "In this environment, our 3D micro-cleaning proves its worth before the final painting. Many well-known manufacturers use our special cleaning procedure with the linear-brush robot. “
In the Wandres technical research center, endurance tests are conducted with a multi-axis robot, which inspects the cleaning quality and results of the special brush in different surface structures. The linear-brush robot is ideal for cleaning complex geometrical shapes, which are usually not accessible with alternative methods. Edges and beads can be optimally cleaned with appropriate programming. The travel speed of the robot amounts to about 300 to 400 mm/s.
Both cyclic and continuous operations are possible. Linear-brush robots are used mainly in primer and top coat lines in the automotive industry.
But plastic parts such as bumpers can also be cleaned as a preliminary measure to the painting before the flame impingement during the process. Basis of the operation is the patented "Ingromat" process of the company. It is a special damp mopping process.
Cleaning systems for the automotive industry: The 6-axis robot with the industrial linear brush from Wandres is at work day and night in the technical research center. All axes are equipped with various energy supply systems, so that the cables withstand the demanding movements.
With it, the frequently occurring electrostatic charges can be minimized considerably and adhering dust and particles removed safely. In addition, the linear brush has a flexibly mounted working run that adapts perfectly to the convex and concave curved surfaces. The deviation tolerance of the linear brush is -30 / +10 mm, relative to the surface plane. The pressure can be controlled individually.
On axis 1, the rotation axis, the energy supply system "twisterchain®" proves its worth. Here it is used in a rotation of 180°.
The 6-axis robot has now been operating at the technical research center for over two and a half years. "Originally, all robot cables were protected against mechanical damage by protective hoses provided at the factory," recalls Martin Weber. "But this didn't work. They were constantly torn or frayed, with the result that the entire test plant came to a standstill. Therefore we were looking for a technical solution that protects the various cables safely and permanently. " In almost all the Wandres cleaning systems for the various industries, energy chains® from the comprehensive modular kit are used. This modular kit for virtually any energy supply includes about 80,000 components. In this case, all six axes are equipped with various three-dimensionally moving energy chains®, specifically designed for demanding robotic applications.
The compact "triflex® RS" set is used on the axes 4 to 6. With this universal module, the energy chain® is always routed parallel to the robot arm saving space.
In the circular movement of the axis 1, the axis of rotation, a "twisterchain®" proves its worth.
This spiral-shaped modular energy supply system is suitable for circular movements up to 540° and can be configured online. On the axes 2 to 6, the multi-dimensionally moving energy supply systems from the large "triflex® R" family display their strengths. This quick-mounting hose packets for the robot industry reduce downtimes, provide stability and safety; from large welding robots to small palletizing robots. Due to its round design, the chain glides over the outer contour of the robot and doesn't get wedged or hooked. The smooth inner contour moreover extends the lifetime of the routed cables many times over.
The axes 2 and 3 of the Wandres robot are equipped with the particularly easy to handle option "triflex® R light" . This is a functionally reliable solution for less complex movements. In contrast, the compact "triflex® RS" set is used on the axes 4 to 6. With this universal module, the energy chain® is always routed parallel to the robot arm saving space. The module can be mounted directly on all mounting points of the robot. In this case, the so-called "Easy" design was selected for the quick pressing-in of the cables and hoses by hand. The cables in this option are always visible and accessible from the outside, so that repairs can be done very quickly.
By its modular design with individual elements, the multi-dimensional movable "triflex® R" robot chains can always be adjusted in length any time. A shortening and lengthening is possible at any point. Martin Weber of Wandres: "As we conduct new tests or the requirements of our customers vary always, it is of course important to have the ability to adjust the energy supply systems easily. " Even the replacement or retrofitting of a single cable, or an entire cable packet is easily done on the robot without taking much time, because the chains can be quickly filled from the outside.
Energy supply system "triflex® R" with integrated retaining spring. This always generates a directed pretension to prevent stress on cables.
The 6-axis robot in the technical research center is at work day and night. Martin Weber: "The energy supply systems must at all times withstand the most varied movement sequences of the linear brush. " In addition, there is the multitude of stored programs. Generally, the batch size 1 prevails in the painting line of the automotive industry. As part of the simulation, Wandres therefore tests different software solutions, which in turn have an impact on the movements of the robot.
Neat connection of the brush robot to the energy supply system. The bus cable (purple) is a special cable for dynamic use in energy chains®.
igus® contact+49 (0) 2203-9649-0Send e-mail to igus®
Product finderOnline catalogApplication examplesNews 2013Design and Selection Tools3D-CADProduct comparisonService life calculationShelving configuratorSpecification of
E-Chains®3D CAD configurator for E-Chains® with circular motionTwisterChain®
3D CAD configurator for spiral E-Chains®Email the product expertDesign informationAssembly InstructionsInquiry/orderQuickSpecPart No. searchCatalogs/samplesDownload